/**
 *
 *  The "params" is a single object that can have the following properties:
 *
 *    prop. name   | description
 *  -------------------------------------------------------------------------------------------------
 *   inputField    | the ID of an input field to store the date
 *   displayArea   | the ID of a DIV or other element to show the date
 *   button        | ID of a button or other element that will trigger the calendar
 *   eventName     | event that will trigger the calendar, without the "on" prefix (default: "click")
 *   ifFormat      | date format that will be stored in the input field
 *   daFormat      | the date format that will be used to display the date in displayArea
 *   singleClick   | (true/false) wether the calendar is in single click mode or not (default: true)
 *   firstDay      | numeric: 0 to 6.  "0" means display Sunday first, "1" means display Monday first, etc.
 *   align         | alignment (default: "Br"); if you don't know what's this see the calendar documentation
 *   range         | array with 2 elements.  Default: [1900, 2999] -- the range of years available
 *   weekNumbers   | (true/false) if it's true (default) the calendar will display week numbers
 *   flat          | null or element ID; if not null the calendar will be a flat calendar having the parent with the given ID
 *   flatCallback  | function that receives a JS Date object and returns an URL to point the browser to (for flat calendar)
 *   disableFunc   | function that receives a JS Date object and should return true if that date has to be disabled in the calendar
 *   onSelect      | function that gets called when a date is selected.  You don't _have_ to supply this (the default is generally okay)
 *   onClose       | function that gets called when the calendar is closed.  [default]
 *   onUpdate      | function that gets called after the date is updated in the input field.  Receives a reference to the calendar.
 *   date          | the date that the calendar will be initially displayed to
 *   showsTime     | default: false; if true the calendar will include a time selector
 *   timeFormat    | the time format; can be "12" or "24", default is "12"
 *   electric      | if true (default) then given fields/date areas are updated for each move; otherwise they're updated only on close
 *   step          | configures the step of the years in drop-down boxes; default: 2
 *   position      | configures the calendar absolute position; default: null
 *   cache         | if "true" (but default: "false") it will reuse the same calendar object, where possible
 *   showOthers    | if "true" (but default: "false") it will show days from other months too
 *
 *	Tous ces param?tres sont requis!!!
 *	ils ont ous des valeurs par defaut, N?anmoins, si vous decidez de ne rien passer ? certain param?tres
 *	vous risquez d'avoir des warnings...
 */
Calendar.setup = function (langue, params) {
	function param_default(pname, def) { if (typeof params[pname] == "undefined") { params[pname] = def; } };

	param_default("inputField",     null);
	param_default("displayArea",    null);
	param_default("button",         null);
	param_default("eventName",      "click");
	if(langue == "fr")
	{
		param_default("ifFormat",       "%d/%m/%Y");
		param_default("daFormat",       "%d/%m/%Y");
	}
	else
	{
		param_default("ifFormat",       "%m/%d/%Y");
		param_default("daFormat",       "%m/%d/%Y");
	}
	param_default("singleClick",    true);
	param_default("disableFunc",    null);
	param_default("dateStatusFunc", params["disableFunc"]);
	param_default("firstDay",       0); // Par d?faut c le dimanche qui prend la main (et ouai --> jour de repos)
	param_default("align",          "Br");
	param_default("range",          [1900, 2999]);
	param_default("weekNumbers",    true);
	param_default("flat",           null);
	param_default("flatCallback",   null);
	param_default("onSelect",       null);
	param_default("onClose",        null);
	param_default("onUpdate",       null);
	param_default("date",           null);
	param_default("electric",       true);
	param_default("step",           2);
	param_default("position",       null);
	param_default("cache",          false);
	param_default("showOthers",     false);

	var tmp = ["inputField", "displayArea", "button"];
	for (var i in tmp) {
		if (typeof params[tmp[i]] == "string") {
			params[tmp[i]] = document.getElementById(params[tmp[i]]);
		}
	}
	
	if (!(params.flat || params.inputField || params.displayArea || params.button)) {
		alert("Calendar.setup:\n  Rien ? installer (aucun parametre trouv?).");
		return false;
	}

	function onSelect(cal) {
		var p = cal.params;
		var update = (cal.dateClicked || p.electric);
		if (update && p.flat) {
			if (typeof p.flatCallback == "function")
				p.flatCallback(cal);
			else
				alert("No flatCallback given.");
			return false;
		}
		if (update && p.inputField) {
			p.inputField.value = cal.date.print(p.ifFormat);
			if (typeof p.inputField.onchange == "function")
				p.inputField.onchange();
		}
		if (update && p.displayArea)
			p.displayArea.innerHTML = cal.date.print(p.daFormat);
		if (update && p.singleClick && cal.dateClicked)
			cal.callCloseHandler();
		if (update && typeof p.onUpdate == "function")
			p.onUpdate(cal);
	};

	if (params.flat != null) {
		if (typeof params.flat == "string")
			params.flat = document.getElementById(params.flat);
		if (!params.flat) {
			alert("Calendar.setup:\n  Flat specified but can't find parent.");
			return false;
		}
		var cal = new Calendar(params.firstDay, params.date, params.onSelect || onSelect);
		cal.params = params;
		cal.weekNumbers = params.weekNumbers;
		cal.setRange(params.range[0], params.range[1]);
		cal.setDateStatusHandler(params.dateStatusFunc);
		cal.create(params.flat);
		cal.show();
		return false;
	}

	var triggerEl = params.button || params.displayArea || params.inputField;
	triggerEl["on" + params.eventName] = function() {
		var dateEl = params.inputField || params.displayArea;
		var dateFmt = params.inputField ? params.ifFormat : params.daFormat;
		var mustCreate = false;
		var cal = window.calendar;
		if (!(cal && params.cache)) {
			window.calendar = cal = new Calendar(params.firstDay,
							     params.date,
							     params.onSelect || onSelect,
							     params.onClose || function(cal) { cal.hide(); });
			cal.weekNumbers = params.weekNumbers;
			mustCreate = true;
		}
		cal.showsOtherMonths = params.showOthers;
		cal.yearStep = params.step;
		cal.setRange(params.range[0], params.range[1]);
		cal.params = params;
		cal.setDateStatusHandler(params.dateStatusFunc);
		cal.setDateFormat(dateFmt);
		if (mustCreate)
			cal.create();
		//	alert(params.inputField.value);
		cal.parseDate(dateEl.value || dateEl.innerHTML);
		cal.refresh();
		if (!params.position)
			cal.showAtElement(params.button || params.displayArea || params.inputField, params.align);
		else
			cal.showAt(params.position[0], params.position[1]);
		return false;
	};
};